BRAKE#.SAFE.SBT.ELAPSED

Description

Returns the elapsed milliseconds since the last successful Safe Brake Test (SBT) on the specified brake. When the returned time reaches the max period defined by the safety parameters AXIS#.SAFEPARAM.SBT.MAXTIMEINTERVAL, the Safe Brake Acknowledgment (SBA) signal is set to low.

Code

--> BRAKE1.SAFE.SBT.ELAPSED
3306031

Context

For complete SBT information refer to SBT (Safe Brake Test).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

02-00-00-000

Implemented in SMM revision v0.32

General Information

Type

Read Only
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
BRAKE1.SAFE.SBT.ELAPSED

40f2h

01h

Unsigned32

-

-

Read only

No

BRAKE2.SAFE.SBT.ELAPSED

40f2h

02h

Unsigned32

-

-

Read only

No